ttps://www.automationdirect.com/click-plus-plc
(VID-CL-0066)
The Click PLUS PLC is the newest line of CPUs for the CLICK PLC Family line.
This video details the steps needed to convert your CLICK PLC project to the CLICK PLUS PLC.
In this video, we will show you just how quick and easy it is to connect your PLC to WI-FI.
The CLICK PLUS PLC uses the same FREE PLC programming as the standard CLICK PLC line. Also uses the same CLICKable Stacakble I/O modules as the CLICK PLC.
Download this FREE programming software now, and start saving yourself both time and money.
Our FREE Practical Guide to Programmable Logic Controllers eBook: https://www.automationdirect.com/adc/adcliterature/adcliterature#ebook
Converting your existing CLICK PLC project to a new CLICK PLUS hardware is extremely easy. Let’s say we have this CPU, and now we want a combo wired and wireless option CLICK PLUS CPU. First, go to this page in the CLICK manual and it will show the correct mix of parts to replace your CPU. So, this CPU converts with this expansion module, making the hardware conversion quick and easy. The software side of this could not be simpler. Install version 3.0, or above, of the CLICK programming software. Open up your original project. Here you can select to make a backup copy of your original project, before you make these changes. Select the Function tab. Select the system configuration and here change the CPU and the Slot 0 module to ones that you selected from the manual. And if you have analog, make sure to set those up also. Now, just send this project to your new CPU. And you are ready to go. Just that easy. If you have any question on the CLICK PLC, please feel free to comment below or call our technical support team. CLICK here to see more videos on the CLICK PLC line and click here to subscribe to our YouTube channel for new products and solutions.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings