BRX Do-more CTRIO2 Motion Demo Hardware from AutomationDirect


Related Products

BX-DM1E-M-D
BX-DM1E-M-D Thumbnail
BX-DM1E-M
BX-DM1E-M Thumbnail
BX-DM1-10AR-D
BX-DM1-10AR-D Thumbnail
BX-DM1-10ER-D
BX-DM1-10ER-D Thumbnail
BX-DM1-10ED1-D
BX-DM1-10ED1-D Thumbnail
BX-DM1-10ED2-D
BX-DM1-10ED2-D Thumbnail
BX-DM1E-10AR3-D
BX-DM1E-10AR3-D Thumbnail
BX-DM1E-10ER3-D
BX-DM1E-10ER3-D Thumbnail
BX-DM1E-10ED13-D
BX-DM1E-10ED13-D Thumbnail
BX-DM1E-10ED23-D
BX-DM1E-10ED23-D Thumbnail
BX-RTB10
BX-RTB10 Thumbnail
BX-RTB10-1
BX-RTB10-1 Thumbnail
BX-RTB10-2
BX-RTB10-2 Thumbnail
BX-DM1-18ER-D
BX-DM1-18ER-D Thumbnail
BX-DM1-18ED2-D
BX-DM1-18ED2-D Thumbnail
BX-DM1-18ED1-D
BX-DM1-18ED1-D Thumbnail
BX-DM1E-18ER3-D
BX-DM1E-18ER3-D Thumbnail
BX-DM1E-18ED23-D
BX-DM1E-18ED23-D Thumbnail
BX-DM1E-18ED13-D
BX-DM1E-18ED13-D Thumbnail
BX-DM1-18AR
BX-DM1-18AR Thumbnail
BX-DM1-18ER
BX-DM1-18ER Thumbnail
BX-DM1-18ED2
BX-DM1-18ED2 Thumbnail
BX-DM1-18ED1
BX-DM1-18ED1 Thumbnail
BX-DM1E-18AR3
BX-DM1E-18AR3 Thumbnail
BX-DM1E-18ER3
BX-DM1E-18ER3 Thumbnail
BX-DM1E-18ED23
BX-DM1E-18ED23 Thumbnail
BX-DM1E-18ED13
BX-DM1E-18ED13 Thumbnail
BX-RTB18
BX-RTB18 Thumbnail
BX-RTB18-1
BX-RTB18-1 Thumbnail
BX-RTB03
BX-RTB03 Thumbnail
BX-RTB03-1
BX-RTB03-1 Thumbnail
BX-RTB05
BX-RTB05 Thumbnail
BX-RTB05-1
BX-RTB05-1 Thumbnail
BX-RTB05-2
BX-RTB05-2 Thumbnail
BX-RTB06
BX-RTB06 Thumbnail
BX-RTB06-1
BX-RTB06-1 Thumbnail
BX-DM1-36ER-D
BX-DM1-36ER-D Thumbnail
BX-DM1-36ED2-D
BX-DM1-36ED2-D Thumbnail
BX-DM1-36ED1-D
BX-DM1-36ED1-D Thumbnail
BX-DM1E-36ER3-D
BX-DM1E-36ER3-D Thumbnail
BX-DM1E-36ED23-D
BX-DM1E-36ED23-D Thumbnail
BX-DM1E-36ED13-D
BX-DM1E-36ED13-D Thumbnail
BX-DM1-36ER
BX-DM1-36ER Thumbnail
BX-DM1-36AR
BX-DM1-36AR Thumbnail
BX-DM1-36ED2
BX-DM1-36ED2 Thumbnail
BX-DM1-36ED1
BX-DM1-36ED1 Thumbnail
BX-DM1E-36ER3
BX-DM1E-36ER3 Thumbnail
BX-DM1E-36AR3
BX-DM1E-36AR3 Thumbnail
BX-DM1E-36ED23
BX-DM1E-36ED23 Thumbnail
BX-DM1E-36ED13
BX-DM1E-36ED13 Thumbnail
BX-RTB36
BX-RTB36 Thumbnail
BX-RTB36-1
BX-RTB36-1 Thumbnail
BX-P-SER2-RJ12
BX-P-SER2-RJ12 Thumbnail
BX-P-SER2-TERM
BX-P-SER2-TERM Thumbnail
BX-P-SER4-TERM
BX-P-SER4-TERM Thumbnail
BX-P-USB-B
BX-P-USB-B Thumbnail
BX-P-ECOMLT
BX-P-ECOMLT Thumbnail
BX-RTB03S
BX-RTB03S Thumbnail
BX-08ND3
BX-08ND3 Thumbnail
BX-12ND3
BX-12ND3 Thumbnail
BX-16ND3
BX-16ND3 Thumbnail
BX-08NF3
BX-08NF3 Thumbnail
BX-08TD1
BX-08TD1 Thumbnail
BX-08TD2
BX-08TD2 Thumbnail
BX-12TD1
BX-12TD1 Thumbnail
BX-12TD2
BX-12TD2 Thumbnail
BX-16TD1
BX-16TD1 Thumbnail
BX-16TD2
BX-16TD2 Thumbnail
BX-08CD3R
BX-08CD3R Thumbnail
BX-12CD3D1
BX-12CD3D1 Thumbnail
BX-12CD3D2
BX-12CD3D2 Thumbnail
BX-16CD3D1
BX-16CD3D1 Thumbnail
BX-16CD3D2
BX-16CD3D2 Thumbnail
BX-RTB08
BX-RTB08 Thumbnail
BX-RTB08-1
BX-RTB08-1 Thumbnail
BX-RTB08-2
BX-RTB08-2 Thumbnail
BX-08NB
BX-08NB Thumbnail
BX-12NB
BX-12NB Thumbnail
BX-16NB
BX-16NB Thumbnail
BX-08NA
BX-08NA Thumbnail
BX-12NA
BX-12NA Thumbnail
BX-16NA
BX-16NA Thumbnail
BX-08TA
BX-08TA Thumbnail
BX-12TA
BX-12TA Thumbnail
BX-08TR
BX-08TR Thumbnail
BX-12TR
BX-12TR Thumbnail
BX-16TR
BX-16TR Thumbnail
BX-05TRS
BX-05TRS Thumbnail
BX-08AD-1
BX-08AD-1 Thumbnail
BX-08AD-2B
BX-08AD-2B Thumbnail
BX-08DA-1
BX-08DA-1 Thumbnail
BX-08DA-2B
BX-08DA-2B Thumbnail
BX-04THM
BX-04THM Thumbnail
BX-PGM-CBL
BX-PGM-CBL Thumbnail
BX-DM1-START
BX-DM1-START Thumbnail
BX-DM1E-START
BX-DM1E-START Thumbnail
H2-DM1
H2-DM1 Thumbnail
H2-DM1E
H2-DM1E Thumbnail
H2-DM1E-START
H2-DM1E-START Thumbnail
T1H-DM1E
T1H-DM1E Thumbnail
T1H-DM1
T1H-DM1 Thumbnail
T1H-CTRIO
T1H-CTRIO Thumbnail
T1H-08TDS
T1H-08TDS Thumbnail


To learn more: https://www.automationdirect.com/do-more?utm_source=7ij-7oGdozw&utm_medium=VideoTeamDescription

(VID-DH-0008)

How to use the Do-more PLC and Do-more Designer Software in a DirectLOGIC PLC System. This video covers the details of the hardware setup used in the CTRIO2 Motion and Do-more processor.

Online Support Page: https://community.automationdirect.com/s/?utm_source=7ij-7oGdozw&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

The hardware used in the CTRIO2 Motion Videos looks like this. Starting down here at the PLC, we have a 4 slot 205 base with the Do-more Processor, an input simulator and the new CTRIO2 module. The Servo Motor is driven by a SureStep Motor Driver through this extension cable. Power for the stepper motor is supplied by this SureStep power supply. The Stepper Motor is connected to a threaded screw which moves a carriage mounted on a rail. The NPN proximity sensor detects when the carriage passes and feeds its output back into the CTRIO2 module where we can use it as a limit. I like this little sensor because it has an LED in it that lights up when it detects something. That makes debug a snap. The Encoder is also fed back to the CTRIO module so we can use it to validate positioning. There is 24Vdc supply powering the encoder and proximity sensor which is not shown here. The great thing about this is I didn’t need any other modules in my PLC system. The CTRIO2 handles everything I need. The Ctrio2 even comes with jumpers that you can install on an internal header to tie all the commons together - that really helps clean up the external wiring and makes your life a whole lot easier. For these videos we have tied all of the input commons together and we have tied all of the output Y’s together (we’re using the C’s as the output signals). The best part of this is you can swap out the CTRIO2 module anytime you want because ALL of the configuration information is stored on the Do-more Processor. You don’t have to worry about re-configuring the module when you replace it. Just shove the new one in and turn the PLC on. The Do-more Processor takes care of the rest. Please understand that this hardware was setup just for demo purposes. It is not supported or sold by Automation Direct so please don’t call Tech asking about it and don’t call sales to try and buy one. Also, note that there are no over-travel limits here so please don’t think of this as a complete hardware setup. It is just intended to quickly demonstrate how to use the CTRIO2 functions and the Do-more processor. And, of course, whenever you are doing motion, always start moving things slow, until you can make sure they work and then speed them up when you feel confident when things work the way you expect. We’ll, That’s all there is to the hardware setup we are using. All of the part numbers shown can be purchased at AutomationDirect.com - you’ll really like the prices there AND the free shipping for all orders over $49? We’ll … that just can’t be beat! Be sure to check out the other videos in this series for more on using motion. And as always, please send us any comments you may have, we appreciate the feedback. Spend Less. Do-more. From AutomationDirect.



No data returned!
An error has occurred! Please contact support
Videos Home > BRX Do-more CTRIO2 Motion Demo Hardware from AutomationDirect