https://www.automationdirect.com/enclosure-air-conditioners
(VID-EN-0003)
AutomationDirect has expanded its Stratus™ line of enclosure air conditioners to include 480V models. Heat inside an enclosure can decrease life expectancy in controlling units such as PLCs, HMI, and AC drives. Excessive heat can cause nuisance faults from electrical and electronic components, circuit breakers and fuses. Stratus enclosure air conditioners can help alleviate such problem.
Learn more at: https://www.automationdirect.com/enclosure-air-conditioners
Check out all of our videos at https://www.AutomationDirect.com/Videos
To subscribe: https://www.youtube.com/user/automationdirect?sub_confirmation=1
Facebook: https://www.facebook.com/AutomationDirect
Twitter: https://twitter.com/AutomationDirec
LinkedIn: https://www.linkedin.com/company/automationdirect
**Prices were valid at the time the video was released and are subject to change.
Welcome to Kickstart where you get to see new products here at AutomationDirect. Today I am going to show you our new 480V enclosure air conditioners from our brand: Stratus. We have just added 12 new parts with these Stratus air conditioners in Sizes of 2000btu, 3000 to 4000btu, 5000btu and 6000 to 8000btu units. Enclosure air conditioners are designed for use in applications such as steel, food processing, petro-chemical, cement, paper/pulp, and plastics and more. The accumulation of heat in an enclosure is potentially damaging to electrical and electronic devices. Overheating can shorten the life expectancy of costly electrical components or lead to catastrophic failure. You and I both know that the equipment inside control enclosures needs to be protected from contaminants, over and under voltages as well as heat, humidity and cold temperatures. Air Conditioners excel in cooling applications because they offer closed loop air circulation for a contaminant free environment and optimal cooling under higher ambient temperatures. These new 480v enclosure air conditioners are microprocessor-based and offer digital temperature controllers that perform the functions of controlling the enclosure temperature while monitoring operating limits and refrigerant pressures. Temperature and alarm status are indicated on the front panel in easy-to-read LEDs. The controller also records the maximum and minimum temperatures within the enclosure. Some of the features found in these Stratus air conditioners are: They are Nema 4, 4x and 12 rated. Pre-wired for external alarm monitoring connections CFC-Free refrigerant Anti-short-cycle compressor protection Highly energy-efficient compressors And more! You can find the agency approvals and specs for these new 480V Stratus Air Conditioners on our website at: www.automationdirect.com Don't forget: we sell other size and voltage air conditioners as well as heaters, filter fans and more environmental controls for enclosures. Check back with us often on AutomationDirects websites or on Youtube.com/Automationdirect for more Kickstart videos. If you are watching us on YouTube, please let us know what you think about these new Stratus Air Conditioners or how you plan to use them in your application by dropping us a comment down below. Thanks for watching and we hope to see you again soon.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings