WEG CFW300/320 VFD Switching Between Remote and Local Modes from AutomationDirect


Related Products

CFW300A01P6S1NB20
CFW300A01P6S1NB20 Thumbnail
CFW300A06P0S1NB20
CFW300A06P0S1NB20 Thumbnail
CFW300A01P6S2NB20
CFW300A01P6S2NB20 Thumbnail
CFW300A02P6S2NB20
CFW300A02P6S2NB20 Thumbnail
CFW300A04P2S2NB20
CFW300A04P2S2NB20 Thumbnail
CFW300A06P0S2NB20
CFW300A06P0S2NB20 Thumbnail
CFW300A07P3S2NB20
CFW300A07P3S2NB20 Thumbnail
CFW300A01P6T2NB20
CFW300A01P6T2NB20 Thumbnail
CFW300A02P6T2NB20
CFW300A02P6T2NB20 Thumbnail
CFW300A04P2T2NB20
CFW300A04P2T2NB20 Thumbnail
CFW300A06P0T2NB20
CFW300A06P0T2NB20 Thumbnail
CFW300A07P3T2NB20
CFW300A07P3T2NB20 Thumbnail
CFW300B10P0B2DB20
CFW300B10P0B2DB20 Thumbnail
CFW300B15P2T2DB20
CFW300B15P2T2DB20 Thumbnail
CFW300-CRS232
CFW300-CRS232 Thumbnail
CFW300-CRS485
CFW300-CRS485 Thumbnail
CFW300-CUSB
CFW300-CUSB Thumbnail
CFW300-KHMIR
CFW300-KHMIR Thumbnail
CFW300-IODR
CFW300-IODR Thumbnail
CFW300-IOAR
CFW300-IOAR Thumbnail
CFW300-IOADR
CFW300-IOADR Thumbnail
CFW300-IOAENC
CFW300-IOAENC Thumbnail
CFW300-KFA-S1-S2
CFW300-KFA-S1-S2 Thumbnail
CFW300-KFB-S2
CFW300-KFB-S2 Thumbnail
CFW-WPS
CFW-WPS Thumbnail
CFW300-FAN-A
CFW300-FAN-A Thumbnail
CFW300-FAN-B
CFW300-FAN-B Thumbnail
CFW320A01P6S1NB20
CFW320A01P6S1NB20 Thumbnail
CFW320A02P6S1NB20
CFW320A02P6S1NB20 Thumbnail
CFW320A04P2S1NB20
CFW320A04P2S1NB20 Thumbnail
CFW320A06P0S1NB20
CFW320A06P0S1NB20 Thumbnail
CFW320A01P6S2NB20
CFW320A01P6S2NB20 Thumbnail
CFW320A02P6S2NB20
CFW320A02P6S2NB20 Thumbnail
CFW320A04P2S2NB20
CFW320A04P2S2NB20 Thumbnail
CFW320A06P0S2NB20
CFW320A06P0S2NB20 Thumbnail
CFW320A07P3S2NB20
CFW320A07P3S2NB20 Thumbnail
CFW320A01P6T2NB20
CFW320A01P6T2NB20 Thumbnail
CFW320A02P6T2NB20
CFW320A02P6T2NB20 Thumbnail
CFW320A04P2T2NB20
CFW320A04P2T2NB20 Thumbnail
CFW320A06P0T2NB20
CFW320A06P0T2NB20 Thumbnail
CFW320A07P3T2NB20
CFW320A07P3T2NB20 Thumbnail
CFW320B10P0B2DB20
CFW320B10P0B2DB20 Thumbnail
CFW320B15P2T2DB20
CFW320B15P2T2DB20 Thumbnail
CFW320A01P1T4NB20
CFW320A01P1T4NB20 Thumbnail
CFW320A02P6T4NB20
CFW320A02P6T4NB20 Thumbnail
CFW320A03P5T4NB20
CFW320A03P5T4NB20 Thumbnail
CFW320A04P8T4NB20
CFW320A04P8T4NB20 Thumbnail
CFW320B07P6T4NB20
CFW320B07P6T4NB20 Thumbnail
CFW320C11P0T4NB20
CFW320C11P0T4NB20 Thumbnail
CFW320C14P0T4NB20
CFW320C14P0T4NB20 Thumbnail
CFW320B01P1T4DB20
CFW320B01P1T4DB20 Thumbnail
CFW320B02P6T4DB20
CFW320B02P6T4DB20 Thumbnail
CFW320B03P5T4DB20
CFW320B03P5T4DB20 Thumbnail
CFW320B04P8T4DB20
CFW320B04P8T4DB20 Thumbnail
CFW320B07P6T4DB20
CFW320B07P6T4DB20 Thumbnail
CFW320C11P0T4DB20
CFW320C11P0T4DB20 Thumbnail
CFW320C14P0T4DB20
CFW320C14P0T4DB20 Thumbnail


To learn more: https://www.AutomationDirect.com/drives?utm_source=6lL9SnstJIc&utm_medium=VideoTeamDescription

(VID-DR-0080)

See how to switch between Remote and Local modes. This video shows you step by step exactly how to do it and what to watch out for so you get up and running quickly.

Online Support Page: https://community.automationdirect.com/s/?utm_source=6lL9SnstJIc&utm_medium=VideoTeamDescription

**Please check our website for our most up-to-date product pricing and availability.


Hide Transcript
View Transcript

Suppose you have an application where you need to control the drive run stop remotely from a control room using a digital input. But, when you are at the drive, you want to use the drives built-in HMI keypad to control run stop and you don’t want the control room to start the drive while you are working on it. I would typically refer to this as my remote control and this as my local control, and then I would add a switch to flip between the two modes. So really, remote and local are just two different drive configurations that you can switch between. We could have called them Drive Configuration 1 and Drive Configuration 2, but since most folks use them in a remote local setup like this, they are generically called Remote and Local modes. The truth is, I could store this configuration in Remote mode and this configuration in the Local mode if I wanted to. Maybe at your factory, the drives are considered to be remote from the control room, so the digital run stop is considered the local control and the drive’s HMI is the remote control. The drive really doesn’t care. It all depends on your application and your point of view and how you want to refer to the two different configurations. Remote is one configuration, local is another. How you configure them is up to you. In each one you can configure Run/Stop, the speed control, Forward and Reverse, and Jog. Let’s do the above example where we control the run stop remotely using a digital input and locally via the drive’s HMI keypad. We’ll control the speed of the drive in both configurations from the drive’s HMI keypad. Both configurations will set forward and reverse to forward only and we won’t use any jog. Now, before starting, let’s reset the drive to factory default so we are starting in the same place. I went ahead and entered these motor and ramp parameters for my setup. I’m using the free WPS software and this optional USB comm module for this video to make it easier for you to see what I am doing. You can do everything we are going to do here right from the drive’s built-in HMI if you prefer to do it that way. OK, for local mode we want the keypad to control run stop. So, I’ll search on Local and we see that the local run stop defaults to the HMI keypad, so we don’t need to do anything there. Looks like local mode also defaults to having the speed controlled by the keypad, forward reverse defaults to always forward only and JOG is not used. Those also happen to be exactly what we want to do. Again, even though we are calling it local mode, you can control any of these from any of the remote comm's, digital I/O, etc. Great, Local is done so let’s search on Remote and set that up. Looks like run stop defaults to being controlled by a digital input which is exactly what we want. So that’s fine. The drive speed defaults to analog input control. Let’s change that so we can control the speed from the HMI keypad when in remote mode. Forward and reverse defaults to controlled by a digital input. We want that to be forced to always forward. And jog also defaults to being controlled by digital input. We aren’t using it in this example, so we'll select not used. Ok, we’ve configured the drive operation for both local and remote modes. All that is left, is to switch between them. Parameter 220 controls that and it looks like it defaults to always local. We’re going to have a switch that controls the mode, so let’s change local remote select to being controlled by a digital input. If we search on digital input, we see that digital input 4 isn’t being used, so let’s have that be our local remote selector. I’ve wired these two switches to the drive like this. So, when I am in LOCAL mode, I can start and stop the drive using the drive’s HMI keypad. But not the switch. And when I am in remote mode, I can control the drive from the switch, but not the HMI. Perfect. Also, the drive’s HMI/Keypad controls the speed in both remote and local modes. Exactly what we asked for. Here is a summary of the parameters we used in this video. I’ll include that list in the videos description below, so you can cut and paste it into your own document. Click here to learn more about the CFW300 series of variable frequency drives. Click here to learn about AutomationDirect’s free support options and click here to subscribe to our YouTube channel so you will be notified when we publish new videos.



No data returned!
An error has occurred! Please contact support
Videos Home > WEG CFW300/320 VFD Switching Between Remote and Local Modes from AutomationDirect