https://www.automationdirect.com/do-more?utm_source=2JvmwjvzMs8&utm_medium=VideoTeamDescription (VID-DD-0049)
- This video gives basic information on Using the RUN "RUN Program" instruction in the Do-more Designer software. It presents information that is commonly missed by users. This WILL NOT be a complete tutorial for the instruction but rather a supplement to the help file and customer experience.
** Software Version used in this video: Do-more Designer 2.0.3
Online Support Page: https://community.automationdirect.com/s/?utm_source=2JvmwjvzMs8&utm_medium=VideoTeamDescription
**Please check our website for our most up-to-date product pricing and availability.
This instruction is used to initiate a Program code block. Notice that it is an edge triggered instruction. So once this instruction is triggered the Program code block will be set to run when the controller gets to it as part of the normal execution order. To View or Edit the execution order select this button from your project browser. By default, user-created Programs and Tasks will be executed in the order that they are added to the project. To see if the Program is currently running, turn the all status button on. If the Program code block is showing with a blue highlight. That means it is currently running and will continue to run each scan, or until stopped by ladder logic or the PLC is taken out of run
Voted #1 mid-sized employer in Atlanta
Check out our
job openings