https://www.automationdirect.com/do-more?utm_source=0EBk8afbIEc&utm_medium=VideoTeamDescription (VID-DD-0010)
- This video gives basic information on Using the WX ""Do-more Network Write" instruction in the Do-more designer software. It presents information that is commonly missed by users. This WILL NOT be a complete tutorial for the instruction but rather a supplement to the help file and customer experience.
** Software Version used in this video: Do-more Designer 2.0
Online Support Page: https://community.automationdirect.com/s/?utm_source=0EBk8afbIEc&utm_medium=VideoTeamDescription
This instruction is for Do more to Do more communication only. Each WX instruction can contain up to 50 individual write requests for a total of up to 1000 bytes of data. The WX instruction can write to all of the built-in memory blocks or structures, and any user-created memory blocks but does NOT support writing to any heap items. Typically the UDP will be this, unless the Remote CPU has a secondary Ethernet connection set up in the system configuration. If the Remote CPU is password protected enter that here Click on Insert to select information to transfer and where to store these in the Remote CPU. Notice that this will indicate how close to the 1000 byte limit you are. Please see the help file for more information.
Voted #1 mid-sized employer in Atlanta
Check out our
job openings